![](https://www.tolomatic.com/wp-content/uploads/2022/07/street-lamp-02-retracted_v2-300x170.jpg)
Theater Lamp Post Actuation
Product Family: Pneumatic
Product Used: CC30 Cable Cylinders
Product Type: Standard
Application Requirements:
Stroke: 168” (4.2 m)
Orientation: Vertical
Application Description:
Lamp post to rise out of the floor, on stage, during musical theater performance..
Challenge:
For their upcoming performance of “Singing in the Rain”, the set designers at the Utah theater wanted a lamp post to come out of the floor for a dance number. This was also going to be a wet environment, as it was the key part for the “raining” portion of the program. To make things even tougher, the ideal lamp post was 14 feet tall.
Tolomatic Solution:
The engineering manager at the theater called their local Tolomatic distributor. After a little discussion, they agreed on the idea of using Tolomatic’s Cable Cylinders. The theater had used these in the past – benefiting from their flexibility of mounting and low cost. They hid the actuators inside a set piece, used a compressed air tank, and worked magic with a wireless remote control. Built-to-order at the required 14 ft length (that’s the easy part, Tolomatic can make these in lengths over 23 ft as a standard.) They needed the 3″ bore to get the necessary force, and it required 2 to move the overall weight of the lamp post. With only 4 weeks to design, test and install; Tolomatic’s fast, built-to-order delivery was critical for this project. A special crate was fabricated to ship these long length actuators.
Customer Benefit:
- Pneumatic actuators gave reliable performance in a wet environment.
- The appearance of the lamp post became a “magical” part of the performance.
- The actuators were delivered on time and the entire system worked great.
ARTENT-010-P